I am using SPI for control of an LCD driver chip which uses the standard CS (chip select) plus D/C (data/command).
I don't see a way to assert multiple PCS lines for a frame in the FIFO. Asserting the D/C via GPIO works, but doesn't allow full performance using the FIFO, because the FIFO timing is async from the GPIO.
Any ideas on this? This was a feature of the Kinetis chip I used previously.
thanks
Not a solution specifically, but I worked around this using 9-bit SPI instead of a dedicated D/C chip select. This is a feature of the LCD controller I am using (st7789). The ninth bit of the frame is used to set the D/C value, using only a single CS.