Mimxrt1060-EVK and Zephyr's LED_blinky

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Mimxrt1060-EVK and Zephyr's LED_blinky

1,126件の閲覧回数
prayrit
Contributor I

Hello everyone, 

I am using the MiMXRT1060-EVK and am currently trying to flash Zephyr's LED_blinky example. I have been on the Zephyr thread and have seen some issues with this board and the LED_blinky. It seems that LED0 is not set to the proper LED_GPIO. If anyone has any idea how to move forward or has any idea where to look to fix the problem please reply!!

Thanks

Pray

ラベル(1)
タグ(2)
0 件の賞賛
3 返答(返信)

1,041件の閲覧回数
dleach
NXP Employee
NXP Employee

The problem has been addressed and is in the pending Release v2.4. 

0 件の賞賛

1,057件の閲覧回数
dleach
NXP Employee
NXP Employee

Pray,

I have narrowed down which changeset broke the support. We will work on getting a fix in next week.

The broken code is sensitive to the sequence on how you test it so if you go back to release 2.2 it works fine and if you download broken code without powering off the board it would continue to work.

We can engage on the Zephyr slack for more information.

David

0 件の賞賛

1,057件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Pray, 

I'm not aware of the example that you mentioned, could you please tell me where did you get this example?

Regards, 

Victor 

0 件の賞賛