Max camera resolution i.MX RT can support ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Max camera resolution i.MX RT can support ?

1,035 Views
hiectai
Contributor III

Hello community.
I have project about camera with i.mx rt 1050, and I need to know about max camera resolution i.mx rt can support ?

I looked at the datasheet and related documents but could not find the answer. Please help me.
Thanks in advance

Labels (1)
Tags (1)
3 Replies

830 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi

It depends in the memory buffer used, speed and pixel format that you want, for example, you could have a 1280×720 8bits/pixel rgb format or a 3840x2160 8bits/pixel monochromatic format.

the SDK package included code with the OV7725 VGA camera sensor 640×480 pixels and the MT9M114 HD camera 1296×976 pixels

Regards

830 Views
hiectai
Contributor III

Hi Jorge Antonio Alcala Vazquez

Thank you so much.

0 Kudos

830 Views
hiectai
Contributor III

Anybody can help me?

0 Kudos