MSDK adaptation configuration - ffconf.h

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MSDK adaptation configuration - ffconf.h

Jump to solution
617 Views
Alberto_isorna
Contributor II

Hello, 

  1. Could you explain me what are the behaviours of different configurations of MSDK bellow?
  2. Are they exclusive or I could define several? Is there any documentation about this?
  3. My program uses the SDRAM but reads some data from the SDCARD, what value should I put?

/*---------------------------------------------------------------------------/
/ MSDK adaptation configuration
/---------------------------------------------------------------------------*/
#define RAM_DISK_ENABLE
/* Available options are:
/ RAM_DISK_ENABLE
/ USB_DISK_ENABLE
/ SD_DISK_ENABLE
/ MMC_DISK_ENABLE
/ SDSPI_DISK_ENABLE
/ NAND_DISK_ENABLE */

Best regards,

Alberto.

Labels (1)
0 Kudos
1 Solution
595 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Alberto,

This defines are the different physical drives you can mount depending on your configuration. You should only select one of them as this will be selected when the file system functions are used. With your configuration you should enable SD_DISK_ENABLE.

Best regards,

Felipe

View solution in original post

0 Kudos
1 Reply
596 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Alberto,

This defines are the different physical drives you can mount depending on your configuration. You should only select one of them as this will be selected when the file system functions are used. With your configuration you should enable SD_DISK_ENABLE.

Best regards,

Felipe

0 Kudos