MIMXRT1064EVK "0 available SWD Devices detected" issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIMXRT1064EVK "0 available SWD Devices detected" issue

1,100 Views
zekelandon
Contributor III

I tried downloading pre-built HelloWorld example to get familiar with the board. After build, when I try to connect to via debugging, IDE shows me the "0 available SWD Devices detected" error.

Help me resolve this!

Regards,

Zeke

Labels (1)
0 Kudos
5 Replies

913 Views
zekelandon
Contributor III

I fixed it and I am able to access the board via debugger now.

Regards,

Zeke

0 Kudos

913 Views
marcohaddad
Contributor III

Hello,

How did you solve it? I'm having the same problem.

Thanks!

0 Kudos

913 Views
zekelandon
Contributor III

You need to modify SW7 switch configuration in NXP board

  • Switch SW7: 0010 --> 0001
  • Reboot the board and download program
  • After successful download, reset the switch back to its original position
  • Reboot the board again, and that's it (Now you will be back to working state)

Mark this solution as Helpful and Correct if it works for you

Regards,

Zeke

913 Views
marcohaddad
Contributor III

Hi, Zeke.

The SW7 was already 0001 when I got the no device detected error.

When you say download program, you mean the program I want to debug to be downloaded with the debugger, right?

Well, that's when I get the error, so I never get a successful download...

Best regards,

Haddad

0 Kudos

913 Views
zekelandon
Contributor III

Hi Marco,

I never faced this issue when SW7 position was 0001. As I never faced this before, I do not have a solution readily available.

Regards,

Zeke

0 Kudos