MIMXRT1064 - any differences between 10x10 and 12x12 package sizes?

cancel
Showing results for 
Search instead for 
Did you mean: 

MIMXRT1064 - any differences between 10x10 and 12x12 package sizes?

Jump to solution
229 Views
jason_lo
Contributor II

We previously designed a custom board using MIMXRT1064DVL6A, which is the 10x10 mm package.  Now that the 12x12 mm package is available, we would like to use that instead.  Besides package size, are there any other differences between them?  We have reviewed datasheet and manual and cannot find any differences, but want to double-check.

Regards,

Jason

Labels (1)
Tags (1)
1 Solution
170 Views
FelipeGarcia
NXP TechSupport
NXP TechSupport

Hi Jason,

 

You are correct, there are no differences apart from the package.

 

Best regards,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored.

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

------------------------------------------------------------------------------ 

View solution in original post

1 Reply
171 Views
FelipeGarcia
NXP TechSupport
NXP TechSupport

Hi Jason,

 

You are correct, there are no differences apart from the package.

 

Best regards,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored.

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

------------------------------------------------------------------------------ 

View solution in original post