MIMXRT1060-EVK: Peripherals setting

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIMXRT1060-EVK: Peripherals setting

Jump to solution
961 Views
kenji
Contributor IV

Hi All.

I want to drive BLDC motor using TI's motor driver.
And TI's motor driver needs to setup via SPI.

But MIMXRT1060-EVK's Arduino interface, SPI and PWM use the same pin. So I can't drive the motor driver as default board connection.

kenji_0-1624867526540.png

Therefore, I would like to remove the resistance of the boot mode setting and output the PWM2 signal. Someone knows if there is any problem?

I’m using "evkmimxrt1060_mc_pmsm" sample demo code, and on it,  it looks not read the boot mode pins.

I want to know the effect in case remove the resistance of the boot mode pin.

kenji_0-1624867747356.pngkenji_1-1624867762383.png

 

0 Kudos
1 Solution
952 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @kenji 

You are welcome!

If your question is solved, please help me to mark the correct answer, just to close this case.

Any new questions, welcome to create the new case.

Best Regards,

Kerry

View solution in original post

0 Kudos
3 Replies
956 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @kenji 

    BOOT_MODE pin will determine your boot mode during the reset, so I don't recommend to remove the BOOT_MODE pin pull up or pull down, it will influence the boot mode after you do the reset.

    About the J24 SPI and the PWM conflict, please check the RT1060 reference manual, you can find:

kerryzhou_0-1624874262758.png

kerryzhou_1-1624874301975.png

LPSPI and FLEXPWM has a lot of pins, you can select other pins which is not conflict, not just use J24 pins.

 

Wish it helps you!

If you still have questions about it, please kindly let me know.

Best Regards,

kerry

 

 

954 Views
kenji
Contributor IV

Hi kerryzohou-san

 

Thank you for the information!

I will use another pins.

0 Kudos
953 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @kenji 

You are welcome!

If your question is solved, please help me to mark the correct answer, just to close this case.

Any new questions, welcome to create the new case.

Best Regards,

Kerry

0 Kudos