MIMXRT1052 ETHERCAT EXAMPLE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIMXRT1052 ETHERCAT EXAMPLE

Jump to solution
1,327 Views
omerkaanbasakin
Contributor IV

Hı I am working on MIMXRT1052 in mcuxpresso with SDK_2.7.0_MIMXRT1052xxxxB ETHERCAT example and cannot find in sdk. How can ı get example ?

Labels (1)
0 Kudos
1 Solution
1,219 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Omer Kaan Basakinci ,

   We just have the enet sample code, which can be found from the SDK folder:

SDK_2.7.0_EVKB-IMXRT1050\boards\evkbimxrt1050\driver_examples\enet

  We still don't have the ETHERCAT example, you may need to port it by yourself.

Best Regards,

Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

1 Reply
1,220 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Omer Kaan Basakinci ,

   We just have the enet sample code, which can be found from the SDK folder:

SDK_2.7.0_EVKB-IMXRT1050\boards\evkbimxrt1050\driver_examples\enet

  We still don't have the ETHERCAT example, you may need to port it by yourself.

Best Regards,

Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------