MIMXRT1050-EVK

cancel
Showing results for 
Search instead for 
Did you mean: 

MIMXRT1050-EVK

282 Views
sk2
Contributor I

Hallo guys,

Is it possible to integrate 7 Analog sensor and 5 Digital sensor with MIMXRT1050-EVK evaluation kit? The voltage level of the analog sensors are 0-10 V. I saw that there is Arduino interface available. Do I need an extra daughter board to conenct the output of the sensors in the I/O pin of the evaluation kit? The sensors communicate through I2C.

Thank you.

0 Kudos
1 Reply

191 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

It will depends on how does each sensor communicates. For example, if one of your digital sensors communicates through SPI you will need 4 pins, but if it communicates through I2C you will only need two pins. For the analog sensors, you have the ADC.While working with the MIMXRT1050-EVK you have the ARDUINO Interface pins available to connect. Hope it help you.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos