MIMXRT1020-EVK Power Mode Switch

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIMXRT1020-EVK Power Mode Switch

656 Views
qinxi
Contributor I

Hi,

I'm using iMXRT1020-EVK board.I saw in the datasheet that the power consumption of the RT1021 is only 20uA in the SNVS mode,but I found that the SNVS mode has 20mA in the RT1020-EVK.

RT1021CAF4A 100 pin :How to wake up SNVS mode without wakeup pin?

IDE:MCUXpresso IDE;

SDK:SDK_2.6.1_MIMXRT1021xxxxx;

Labels (1)
0 Kudos
2 Replies

573 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

>>I'm using iMXRT1020-EVK board.I saw in the datasheet that the power consumption of the RT1021 is only 20uA in the SNVS mode,but I found that the SNVS mode has 20mA in the RT1020-EVK.

 Please find the detail power consumption of SNVS mode as the below. Please double check your measure.

pastedImage_1.png

For the SNVS mode how to handle it. Please find it as the link.

URL:https://www.nxp.com/docs/en/application-note/AN12085.pdf?fsrch=1&sr=1&pageNum=1.

Hope it help you.Have a nice day.

 

0 Kudos

573 Views
qinxi
Contributor I

And I found that the program could not be programmed in low power mode.

If I have a program that is powered on and enters a low-power mode (such as SNVS mode), what other methods can be used to wake up the chip in addition to changing the boot mode to erase the flash?

0 Kudos