Hi
We would like to use the MFG tool for mass production of our IMX7 device. I edited the UICfg.ini to use it with four devies
which can be simultaneously attached to multiple USB ports of the host PC and can be programmed simultaneously.
I am able to programme four devices at a time.
Is there any way to increase this further so that I can programme more devices simultaneously which will be very helpful in mass production.
Hi Naresh
seems mfg tool should be modified to support more devices, sources are available on
GitHub - NXPmicro/mfgtools: Freescale/NXP I.MX Chip image deploy tools.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------