MCUXpresso can't connect EVK1050B

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso can't connect EVK1050B

Jump to solution
873 Views
Haber
Contributor I

Hi,

I have got a new EVK1050B and Getting Started as webpage Getting Started with the MIMXRT1050-EVK Evaluation Board | NXP Semiconductors.

My host OS windows 11

MCUXpresso IDE v11.6.0

SDK 2.12

After click 'Debug', happens an error "socketExecption", reason: connection reset.

I have re-installed mcuxpresso and it still happns.

Please help.

 

See details error info below

Connection reset
at java.base/java.net.SocketInputStream.read(Unknown Source)
at java.base/java.net.SocketInputStream.read(Unknown Source)
at java.base/sun.nio.cs.StreamDecoder.readBytes(Unknown Source)
at java.base/sun.nio.cs.StreamDecoder.implRead(Unknown Source)
at java.base/sun.nio.cs.StreamDecoder.read(Unknown Source)
at java.base/sun.nio.cs.StreamDecoder.read0(Unknown Source)
at java.base/sun.nio.cs.StreamDecoder.read(Unknown Source)
at java.base/java.io.InputStreamReader.read(Unknown Source)
at com.nxp.mcuxpresso.core.debug.support.linkserver.redlink.client.RedlinkServerClient.receive(RedlinkServerClient.java:965)
at com.nxp.mcuxpresso.core.debug.support.linkserver.redlink.client.RedlinkServerClient.sendReceive(RedlinkServerClient.java:1068)
at com.nxp.mcuxpresso.core.debug.support.linkserver.redlink.client.RedlinkServerClient.sendReceive(RedlinkServerClient.java:1053)
at com.nxp.mcuxpresso.core.debug.support.linkserver.redlink.client.RedlinkServerClient.sendReceive(RedlinkServerClient.java:1040)
at com.nxp.mcuxpresso.core.debug.support.linkserver.redlink.client.RedlinkServerClient.probeList(RedlinkServerClient.java:950)
at com.nxp.mcuxpresso.core.debug.support.linkserver.emulators.common.RedlinkServerEmuHandler.discoverEmulators(RedlinkServerEmuHandler.java:222)
at com.nxp.mcuxpresso.core.debug.support.linkserver.emulators.win.AbstractWinServerProbe.discoverEmulators(AbstractWinServerProbe.java:72)
at com.nxp.mcuxpresso.core.debug.support.linkserver.emulators.EmulatorsDB.getEmus(EmulatorsDB.java:269)
at com.nxp.mcuxpresso.core.debug.support.linkserver.emulators.EmulatorsDB.getEmulatorInfo(EmulatorsDB.java:209)
at com.nxp.mcuxpresso.core.debug.support.linkserver.emulators.EmulatorsDB.getAvailableEmulators(EmulatorsDB.java:138)
at com.nxp.mcuxpresso.core.debug.support.linkserver.emulators.TargetDiscovery.getAvailableEmulators(TargetDiscovery.java:508)
at com.nxp.mcuxpresso.core.debug.support.linkserver.launch.LinkServerLaunchConfigHandler.probeDiscovery(LinkServerLaunchConfigHandler.java:622)
at com.nxp.mcuxpresso.core.debug.launch.ProbeDiscoveryJob.run(ProbeDiscoveryJob.java:60)
at org.eclipse.core.internal.jobs.Worker.run(Worker.java:63)

 

0 Kudos
1 Solution
865 Views
Haber
Contributor I

Thanks a lot.

According to mcuxpresso user guide, additional driver is installed and the problem is gone. 

See follows

  • CMSIS-DAP firmware installed onto on-board debug probe hardware (as shipped by default on LPCXpresso MAX and CD boards)

    • For more information on LPCXpresso boards see:

    • Additional driver may be required:

View solution in original post

2 Replies
866 Views
Haber
Contributor I

Thanks a lot.

According to mcuxpresso user guide, additional driver is installed and the problem is gone. 

See follows

  • CMSIS-DAP firmware installed onto on-board debug probe hardware (as shipped by default on LPCXpresso MAX and CD boards)

    • For more information on LPCXpresso boards see:

    • Additional driver may be required:

870 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Firstly, I'd like to suggest you'd better check the hardware setup, such as power supply, boot mode, etc.
Next, I'd like to suggest you use the SPT tool to contact the EVK board to verify the external Flash connection.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos