MAX2771 - Read register from SPI with IMX

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MAX2771 - Read register from SPI with IMX

1,427 Views
lacouturepatric
Contributor I

Hello,

I try to configure a MAX2771 component (GNSS receiver) with an IMXRT1064 by SPI. The IMXRT1064 is a master and the MAX277 is a slave.

I succeed in writing into the MAX2771 registers ( 48 bits / frame) by using the sdk exemple (driver_examples\lpspi\interrupt).

I did not succeed in reading the MAX2771 registers . How do I proceed to configure LPSPI to work as follow? 

- The IMX first asserts CSN (low) ,

- Then it transferts address (12 bits) + 1 read bit  and 3 bits to 0,

- Then SDATA is set in tri-stated by the IMX and it generates 32 clk,

- The MAX2771 then starts driving SDATA () and outputting the 32 bits,

- The IMX disasserts CSN (high),

- The IMX read his "RDR register" to have the MAX2771 register value.

Do you have exemples ?

You can find attached "Register Read Functional Timing" figure

Thank you for your help.

Best regards,

Patrice Lacouture

0 Kudos
2 Replies

1,268 Views
lacouturepatric
Contributor I

Hello Mr Garcia,

Thank you.

Regards,

Patrice

0 Kudos

1,268 Views
FelipeGarcia
NXP Employee
NXP Employee

Hello Patrice,

 

I recommend you to check how the masterConfig structure is configured in the example. Here you can change bits per frame, clock polarity, PCS active high or low, etc. according to your device needs.

   lpspi_master_config_t masterConfig;

    /*Master config*/
    masterConfig.baudRate     = TRANSFER_BAUDRATE;
    masterConfig.bitsPerFrame = 8;
    masterConfig.cpol         = kLPSPI_ClockPolarityActiveHigh;
    masterConfig.cpha         = kLPSPI_ClockPhaseFirstEdge;
    masterConfig.direction    = kLPSPI_MsbFirst;

    masterConfig.pcsToSckDelayInNanoSec        = 1000000000 / masterConfig.baudRate;
    masterConfig.lastSckToPcsDelayInNanoSec    = 1000000000 / masterConfig.baudRate;
    masterConfig.betweenTransferDelayInNanoSec = 1000000000 / masterConfig.baudRate;

    masterConfig.whichPcs           = EXAMPLE_LPSPI_MASTER_PCS_FOR_INIT;
    masterConfig.pcsActiveHighOrLow = kLPSPI_PcsActiveLow;

    masterConfig.pinCfg        = kLPSPI_SdiInSdoOut;
    masterConfig.dataOutConfig = kLpspiDataOutRetained;

    srcClock_Hz = LPSPI_MASTER_CLK_FREQ;
    LPSPI_MasterInit(EXAMPLE_LPSPI_MASTER_BASEADDR, &masterConfig, srcClock_Hz);

Best regards,

Felipe

0 Kudos