Hello There,
I want to develop a local speech recognition system which can recognise a limited vocabulary of 30 words with a wake word using i.MX RT106L, can I add my own words to the Local voice SDK, If it is possible how should I proceed, please do let me know.
Hope for a positive response soon
Thank & Regards
Yogesh
Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Can I add my own words to the Local voice SDK, If it is possible how should I proceed, please do let me know?
-- Please contact NXP ( local-commands@nxp.com) to discuss the cost and process to create speech recognition models for custom command sets and wake words. The i.MX RT106L solution can support commands sets containing up to thirty commands, in over sixty different languages.
Hope it helps.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------