LWIP and heap

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LWIP and heap

1,931 Views
mspenard603
Contributor IV

Hi Gents,

iMXRT1062 user. And I'm looking to move LWIP's heap to external ram to save on DTC, as indicated in LWIP's mem.c:

/** If you want to relocate the heap to external memory, simply define
* LWIP_RAM_HEAP_POINTER as a void-pointer to that location.
* If so, make sure the memory at that location is big enough (see below on
* how that space is calculated). */
#ifndef LWIP_RAM_HEAP_POINTER
/** the heap. we need one struct mem at the end and some room for alignment */
LWIP_DECLARE_MEMORY_ALIGNED(ram_heap, MEM_SIZE_ALIGNED + (2U * SIZEOF_STRUCT_MEM));
#define LWIP_RAM_HEAP_POINTER ram_heap
#endif /* LWIP_RAM_HEAP_POINTER */

I want to make sure I do this correctly. My heap is at RAM4 with "End" location. Has anyone been down this road? What exactly do I need to #define ?

linker.png

Untitled.png

0 Kudos
5 Replies

1,791 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello, 

The modification you showed on the image is to change the Heap of the entire application, if you want to change the LWIP Heap, you will need to define LWIP_RAM_HEAP_POINTER as a void-pointer to location 0x80000000.


Have a great day,
Victor

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos

1,791 Views
mspenard603
Contributor IV

Yes, its the entire application heap setup of course. I posted it to disclose my setup.

" if you want to change the LWIP Heap, you will need to define LWIP_RAM_HEAP_POINTER as a void-pointer to location 0x80000000."

That is what I'm asking how to properly do.

0 Kudos

1,791 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Mike, 

You can achieve this with the following: 

void *LWIP_RAM_HEAP_POINTER = (void *) 0x80000000;

Regards, 

Victor 

0 Kudos

1,791 Views
mspenard603
Contributor IV

Thank you. I notice LWIP_PBUF_MEMPOOL is also using a bunch of DTC. Is it possible to move this to BOARD_SDRAM as well?

/*
* A list of pools of pbuf's used by LWIP.
*
* LWIP_PBUF_MEMPOOL(pool_name, number_elements, pbuf_payload_size, pool_description)
* creates a pool name MEMP_pool_name. description is used in stats.c
* This allocates enough space for the pbuf struct and a payload.
* (Example: pbuf_payload_size=0 allocates only size for the struct)
*/
LWIP_MEMPOOL(PBUF, MEMP_NUM_PBUF, sizeof(struct pbuf), "PBUF_REF/ROM")
LWIP_PBUF_MEMPOOL(PBUF_POOL, PBUF_POOL_SIZE, PBUF_POOL_BUFSIZE, "PBUF_POOL")

0 Kudos

1,791 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Mike, 

Yes, it is possible to move this to the external SDRAM. 

Regards, 

Victor 

0 Kudos