LVGL acceleration wtih PXP or VGLite?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LVGL acceleration wtih PXP or VGLite?

1,625 Views
erikraynolds
Contributor III

Can be LVGL accelerated with VGLite or PXP on iMX RT1170 device and how?

Can you share the sample code?

 

Thank you.

0 Kudos
2 Replies

1,620 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Can be LVGL accelerated with VGLite or PXP on iMX RT1170 device and how?
-- Yes.
2) Can you share the sample code?
-- Please refer to the LVGL demos in the SDK library.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos

909 Views
Wobaffet
Senior Contributor I
Hello, RT117x MCU's have both, so which one to use and when to use is suggested by NXP? I've checked the GUI_Guider_User_Manual chapter 6 about graphics accelerators but not much information was given in that guide.
0 Kudos