LQFP100 RT1021 Ethernet interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LQFP100 RT1021 Ethernet interface

488 Views
Soos
Contributor II

Hi,

I am using 100-pin MIMXRT1021CAF4A and want to interface Ethernet PHY chip.

I see that ENET_MDIO & ENET_MDC pins are shared with JTAG pins.

In 144-pin package these pins are dedicated.

Evaluation kit schematic uses 144-pin package.

I just want to confirm that I have to share these two pins with JTAG ?

Thanks

Suhas

Labels (1)
0 Kudos
1 Reply

452 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi Suhas,

Yes, you have to share the pin. If you don't want share, you can use SWD debug instead of JTAG. GPIO_AD_B0_04 and GPIO_AD_B0_05 is not used by SWD.

Regards,

Jing

0 Kudos