LPSPI how to set for QSPI flash device

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPSPI how to set for QSPI flash device

ソリューションへジャンプ
1,170件の閲覧回数
fredfu
NXP Employee
NXP Employee

Hi,

   I see the RM of RT1060, as if the LPSPI module can support QSPI device, but it is very simply described in RM, and there is no example for the usage in SDK, the LPSPI module can support QSPI device? Thanks.

Best Regards,

Fred Fu

0 件の賞賛
1 解決策
1,152件の閲覧回数
fredfu
NXP Employee
NXP Employee

Hi Mark,

     Thanks for your confirm.

Best Regards,

Fred Fu

元の投稿で解決策を見る

0 件の賞賛
2 返答(返信)
1,165件の閲覧回数
mjbcswitzerland
Specialist V

Hi

The LPSPI can be used in Quad data mode by configuring the WIDTH field of the transmit command register for 4-bit transfer (which can be done on a per-transaction basis).
The LPSPI pins use their data functions in this case

 

mjbcswitzerland_0-1604490023944.png

QSPI flash devices can usually operate in single-bit mode so the LPSPI can also operate in standard 1 bit mode with them too if the data rate is not critical.

Regards

Mark
[uTasker project developer for Kinetis and i.MX RT]
Contact me by personal message or on the uTasker web site to discuss professional training, solutions to problems or product development requirements

 

0 件の賞賛
1,153件の閲覧回数
fredfu
NXP Employee
NXP Employee

Hi Mark,

     Thanks for your confirm.

Best Regards,

Fred Fu

0 件の賞賛