LCD Panel rotation (720x1280)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LCD Panel rotation (720x1280)

556 Views
erikraynolds
Contributor III

Per today display examples there is set panel size as 

#define DEMO_PANEL_WIDTH (720)
#define DEMO_PANEL_HEIGHT (1280)

can be DEMO_PANEL_RK055MHD091 rotate? So its Width is 1280 and Height is 720?

0 Kudos
1 Reply

537 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To provide the fastest possible support, I'd highly recommend you to refer to the post.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos