KeyBlob secure boot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

KeyBlob secure boot

883 次查看
otaissey
Contributor III

Hello community,

I am checking the operation of the i.MXRT600 OTFAD boot.

[Question]
Q1.
If the Key written to the shadow register of the i.MX6xx and the KeyBlob written of the QSPI Flash are successfully authenticated, the boot is successful. Is my understand correct ?
Q2.
I have a question about KeyBlob(0x0). the keyBlob is changed in the secure binary built image with SPT, even though the key is the same. How can I understand this ?
I attached file. (FILE NAME: 220429_KeyBlob_v2.pdf)
Please help you understand my question.

Best Regards,
Issey

标签 (1)
0 项奖励
1 回复

861 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To provide the fastest possible support, I'd highly recommend you refer to the application to learn the details on the OTFAD module.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励