Is there an SVD file for i.MXRT1050?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there an SVD file for i.MXRT1050?

Jump to solution
4,156 Views
yrashk
Contributor II

Hi, I am trying to find an SVD file for i.MXRT1050, but so far my search yielded no results. I am intending to use it to create a Rust programming language library for it using svd2rust. Any help will be highly appreciated!

0 Kudos
1 Solution
3,517 Views
b36401
NXP Employee
NXP Employee

I just sent you the files.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
11 Replies
3,517 Views
b2c
Contributor I

Is there an SVD file for the 1050?  (The responses here refer to the 1052 and the 1051--I'm not sure what the differences are from the 1050 that I have...)  

0 Kudos
3,517 Views
mikerob
Contributor I

I would also like the SVD file for i.MXRT1050. There may be others looking for it too.

Where can it be found?

Thanks,

Mike

0 Kudos
3,517 Views
yrashk
Contributor II

Michael,

You can find one for 1052 here GitHub - yrashk/imxrt1052: i.MX RT 1052 for Rust 

I also have one for 1051 from Victor. Let me know if you need that one instead.

Yurii.

3,518 Views
b36401
NXP Employee
NXP Employee

I just sent you the files.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
1,173 Views
auftrag2021
Contributor III

Hi, will the SVD be provided only "privately"?

Would you please provide me the svd file for iMXRT1176, I need it to import into the segger ozone tools

0 Kudos
2,565 Views
wcbdev
Contributor II

Hello,

Can you please also share the .svd files for the IMXRT1064 and IMXRT1062?

0 Kudos
2,466 Views
wcbdev
Contributor II

following up on this ^. Thank you !

0 Kudos
3,516 Views
yrashk
Contributor II

Hi Victor,

I haven't received the files here at the community website. Is there any other way to get the files?

Thank you!

Yurii.

0 Kudos
3,516 Views
b36401
NXP Employee
NXP Employee

It seems there is something wrong with attachments.
Please create a technical case:
https://community.nxp.com/thread/381898
I will send the files over that system.

Have a great day,
Victor

0 Kudos
3,516 Views
yrashk
Contributor II

Victor,

Thank you very much. I created a case 00161398.

Thank you!

Yurii.

0 Kudos
3,516 Views
b36401
NXP Employee
NXP Employee

I sent the files there.