Is there a good example of the use of RT105X MQS?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there a good example of the use of RT105X MQS?

1,661 Views
john_h_holste
Contributor II

We are looking to use MQS to generate some tones in our system directly from a const array in flash. 

Labels (1)
3 Replies

1,295 Views
kellli01
Contributor II

Can I get permission on this link?

https://community.nxp.com/message/1005849

1,295 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

About the example code of MQS, It runs on RT1050 EVB, and is based on SDK_2.3.0_EVK-MIMXRT1050. To build and run the demo, extract the archive file into the directory SDK_2.3.0_EVK-MIMXRT1050\boards\evkmimxrt1050\user_apps. And replace the driver file SDK_2.3.0_EVK-MIMXRT1050\devices\MIMXRT1052\drivers\fsl_sai_edma.c with the attached one to fix a bug. About the example code you can get them here https://community.nxp.com/message/1005849.

1,295 Views
john_h_holste
Contributor II

Hi Rita,

I am not allowed to the what is in the link.. not sure if it is a me thing or a community thing.  Does the example you provide allow the creation of the tones or just pipe an input to an output?

thanks again,

John 

0 Kudos