Is there FreeRTOS, FatFS and LWIP for i.MX RT1050?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there FreeRTOS, FatFS and LWIP for i.MX RT1050?

3,107 Views
milankolar
Contributor I

Hello.

We are using STM32F4 with FreeRTOS, FatFS and LWIP. We are thinking to use i.MX RT1050. Is there this port (FreeRTOS, FatFS and LWIP) for this device? Is there another free similar library?

Thanks. Milan Kolar

Labels (1)
3 Replies

1,521 Views
asick
Contributor III

I'm using RT1050 EVK- i want to know how to build freeRtos application with armgcc linux host machine and copy into sd card and how to get serial console application output(Ex: Hello word).

1,521 Views
turkersezgin
Contributor III

Maybe, there is a person who knows solution :smileyhappy:

0 Kudos

1,521 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Milan,

the SDK for iMXRT includes FreeRTOS with lwip and FATFS. You can build your SDK here Welcome to MCUXpresso | MCUXpresso Config Tools 

Please select SDK builder and then iMXRT


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos