Is possible let RT1050 be AP and station mode simultaneously?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is possible let RT1050 be AP and station mode simultaneously?

858 Views
yen_chen
Contributor III

I use RT1050 WIFI example : wifi_cli.

Can RT1050 be station and AP mode simultaneously?

When RT1050 as AP can let device access but it can't ping google.

How do I set router let another can access?

0 Kudos
5 Replies

837 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Yen:

 

From the release note,  RT1050 can act as AP and STA simultaneously.

danielchen_0-1612617738337.png

Regards

Daniel

0 Kudos

798 Views
yen_chen
Contributor III

Hi @danielchen 

Whether you can ping another router or not when you use AP mode ?

I can use AP mode but I can't ping google. 

Although it support AP ,but it can't share internet.

when I use device connect to RT1050 wifi example code like wifi_cli , wifi iperf,can not ping another router.

Could you check this problem,thanks.

Br,

Yen

0 Kudos

782 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Yen:

 

Sorry ,  I missed your update. I am reproducing your issue.  and  will reply to you later.

About the  AP and STA work in parallel,  they have to stay in the same channel. You can follow up guide to configure STA and AP separately.   AP should switch channel automatically when STA changes channel.

 

Regards

Daniel

0 Kudos

762 Views
danielchen
NXP TechSupport
NXP TechSupport

 Ping google.com from the STA or AP there should be network bridge between RT AP and Ethernet.

Currently, in default demo this support is not there.

0 Kudos

820 Views
yen_chen
Contributor III

Hi @danielchen 

Thank you ,got it.

But when I  use device as AP and then share the internet to another device,it only can ping internal .

I think that is router failed.

What should I do to solve this problem ? 

 

0 Kudos