Is RTCESL library royalty free for the commercial application?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is RTCESL library royalty free for the commercial application?

Jump to solution
850 Views
jamesli
Contributor III

Is RTCESL library royalty free for the commercial application? If license is required, how to obtain it? Any source code disclosed or release for AMCLIB library?

1 Solution
807 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello

You can download it from the website Real Time Control Embedded Software Motor Control and Power Conversion Libraries | NXP . It is the free if you can download directly. 

 Hope it help you. Have a nice day.

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

View solution in original post

1 Reply
808 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello

You can download it from the website Real Time Control Embedded Software Motor Control and Power Conversion Libraries | NXP . It is the free if you can download directly. 

 Hope it help you. Have a nice day.

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------