Interfacing 'eLCDIF Parallel RGB LCD with NXP i.mxrt 1176'

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Interfacing 'eLCDIF Parallel RGB LCD with NXP i.mxrt 1176'

544 Views
Usharani_1
Contributor II

Hi,

We use customized board with NXP i.mxrt1173 MCU.

Tried to interface 'eLCDIF Parallel RGB LCD (800 x 480)', but 'LCD interrupt is not triggering'.

The same LCD works fine with 1060 EVK board using eLCDIF.

The 'SDK' for i.mxrt 1170 have sample code for eLCDIF, but configured for MIPI.

Can anyone upload any sample code or steps to include like the respective clock configuration, pin configuration, driver and support files (eLCDIF parallel RGB LCD using NXP i.mxrt 1176 along with DCD (SDRAM) file) if they have come across a solution for the same.

Thanks

 

0 Kudos
1 Reply

525 Views
CarlosGarabito
NXP TechSupport
NXP TechSupport

Hi @Usharani_1 

We have the next Aplication Note, Use Case of RT1170 LCD Display System based on MIPI DSI https://www.nxp.com/docs/en/application-note/AN12940.pdf

 

Or you can check this excellent blog from a chinese parther https://blog.csdn.net/Oushuwen/article/details/110547413

https://www.cnblogs.com/zhugeanran/p/16218486.html

 

Or this other excellent blog from Erich Styger a https://mcuoneclipse.com/2018/08/12/tutorial-open-source-embedded-gui-library-littlevgl-with-i-mx-rt...

 

0 Kudos