Integration of Keil MDK Middleware in MCUXpresso

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Integration of Keil MDK Middleware in MCUXpresso

跳至解决方案
680 次查看
markus_winkhoef
Contributor II

Hello NXP Community,

is it possible to integrate the Keil MDK Middleware package into the MCUXpresso IDE?

Best regards,

Markus

0 项奖励
1 解答
619 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi Markus,

 

Unfortunately, there is no direct way to do that. If you like to import a Keil project to MCUXpresso the best way is to create a new MCUXpresso project, and then copy the files of the application to that new project.

 

Best regards,

Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
620 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi Markus,

 

Unfortunately, there is no direct way to do that. If you like to import a Keil project to MCUXpresso the best way is to create a new MCUXpresso project, and then copy the files of the application to that new project.

 

Best regards,

Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------