Integration of Keil MDK Middleware in MCUXpresso

cancel
Showing results for 
Search instead for 
Did you mean: 

Integration of Keil MDK Middleware in MCUXpresso

Jump to solution
411 Views
markus_winkhoef
Contributor II

Hello NXP Community,

is it possible to integrate the Keil MDK Middleware package into the MCUXpresso IDE?

Best regards,

Markus

0 Kudos
1 Solution
350 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Markus,

 

Unfortunately, there is no direct way to do that. If you like to import a Keil project to MCUXpresso the best way is to create a new MCUXpresso project, and then copy the files of the application to that new project.

 

Best regards,

Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

1 Reply
351 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Markus,

 

Unfortunately, there is no direct way to do that. If you like to import a Keil project to MCUXpresso the best way is to create a new MCUXpresso project, and then copy the files of the application to that new project.

 

Best regards,

Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------