In application programming aborted due to an out of bounds address.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

In application programming aborted due to an out of bounds address.

1,144 Views
heelcurve5
Contributor II

I have a MIM XRT 1010 eval board and I managed to get it stuck in bootloader mode

When I  plug it in the "Maintenance" drive appears but the COM port does not enumerate.

 I followed instructions in the HELP_FAQ.HTM tried to flash the board with 3 firmware images suggested in the document. (current and 2 older ones). All fail with the error "In application programming aborted due to an out of bounds address"

The images I tried: 

0241_kl26z_microbit_0x8000.hex ,0250_kl26z_microbit_0x8000.hex and 0253_kl26z_microbit_0x8000.hex. 

All failed with the error above.

Where can I get the firmware image for this board? Here are the contents of DETAILS.TXT file on the MAINTENANCE drive

# DAPLink Firmware - see https://mbed.com/daplink
Unique ID: 00000000161321cf00000000000000000000000097969905
HIC ID: 97969905
Auto Reset: 0
Automation allowed: 1
Overflow detection: 0
Daplink Mode: Bootloader
Bootloader Version: 0244
Git SHA: 8ede6eacbce0a3012a899ba13fafe7d400094883
Local Mods: 0
USB Interfaces: MSD
Bootloader CRC: 0xe493996b
Interface CRC: 0x619d86db
Remount count: 3

Thank you 
Andy

Labels (4)
2 Replies

1,046 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello, Andy 

I'm not sure I understood correctly, please correct me if I'm wrong, are you looking to get the firmware for the onboard debugger? 

Regards, 

Victor 

1,046 Views
heelcurve5
Contributor II

Yes I got that sorted out

I downloaded the debugger firmware from this link

https://www.nxp.com/design/microcontrollers-developer-resources/ides-for-kinetis-mcus/opensda-serial...

and it works now

Thank you

Andy

On Wed, Dec 4, 2019 at 9:16 AM victorjimenez <admin@community.nxp.com>