Hello
I am trying to interface a 16 bit 100MSPS parallel ADC with the Flexio port of imxrt1176. Is this feasible?
kind regards
Vinod Ganesh
Solved! Go to Solution.
Hi,
Thanks for your reply.
The FlexIO clock frequency of i.MX RT can up to 120 MHz.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Is this feasible?
-- In my opinion, it's feasible.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Thank you for the information. Could you also confirm that the maximum flexio clock which is 120MHZ as per reference manual is also the maximum parallel port speed possible?
Hi,
Thanks for your reply.
The FlexIO clock frequency of i.MX RT can up to 120 MHz.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------