IMXRT1170 EVK : SW7 not working.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMXRT1170 EVK : SW7 not working.

Jump to solution
744 Views
AndyCapon
Contributor II

Hi Guys,

I don't seem to be having much luck with getting anything from SW7 on my board.

Just to check I wasn't doing something stupid I had a search in the examples and found ewm_c7, in that example SW7 also doesn't work for me.

Can someone with this board please run the ewm_c7 sample and see if it works for them, I'm thinking maybe my board has an issue.

Many thanks

Andy

0 Kudos
1 Solution
709 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi AndyCapon,

  Thanks for your updated information and let me know you are working now.

   If you have any new questions in the future, welcome to create the new question post, thanks.

Wish it helps you!

If you still have questions about it, please kindly let me know!

Best Regards,

Kerry

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

-----------------------------------------------------------------------------

View solution in original post

0 Kudos
3 Replies
728 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi AndyCapon,

I have tested it on my side, it works ok:

kerryzhou_0-1615184124553.png

When you rn the ewm_cm7 project, can you enter the debugger mode or not?

Please note, J38, connect 5-6.

The USB port use J11 which is the debugger port.

Please try it on your side, my SW7 works OK.

 

Wish it helps you!

If you still have questions about it, please kindly let me know.

Kerry

 

719 Views
AndyCapon
Contributor II

Hi Kerry,

Thanks very much for the reply.

I was running with the debugger and uart.

I have just tried again now I know it should work and I managed to get the button to fire off a couple of times by repeatedly clicking it!

So I used some wire to connect the button pins and with that I can trigger it perfectly.

I will desolder the button and solder a replacement on.

 

Thanks for the help.

Andy

 

 

0 Kudos
710 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi AndyCapon,

  Thanks for your updated information and let me know you are working now.

   If you have any new questions in the future, welcome to create the new question post, thanks.

Wish it helps you!

If you still have questions about it, please kindly let me know!

Best Regards,

Kerry

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

-----------------------------------------------------------------------------

0 Kudos