IMXRT1060 and OCOTP shadow registers

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMXRT1060 and OCOTP shadow registers

832 次查看
g_volokh
Contributor I

Hi All.

I am working with IMXRT1060 and see that it has OTP Fuses in the address range 0x400..0x8CF.

The OCOTP works with OTP Fuses via shadow registers. Shadow registers have the address range 0x0000..0x003F.

Question:

- how does one relate to other?

- OCOTP can read, reload and write to/from shadow registers, but how can I write to OTP Fuses?

Thanks and regards,

George Volokh.

0 项奖励
1 回复

733 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) How does one relate to others?
-- The relation between the Fuse and shadow register like the below show.
pastedImage_2.png
fuse_address = fuse_index * 0x10 + 0x400
2) OCOTP can read, reload and write to/from shadow registers, but how can I write to OTP Fuses?
-- Please learn it by referring to 23.4.1.2 Fuse and Shadow Register Read and 23.4.1.3 Fuse and Shadow Register Writes sections in the RM.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励