IMXRT1050 noncached RAM above 0x20240000 for DMA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMXRT1050 noncached RAM above 0x20240000 for DMA

794 Views
jackking
Senior Contributor I

I am trying to configure an area of FlexRAM for DMA buffers in MCUXpresso IDE 11.0 for the i.MXRT1050/1060

When I choose the starting address as 0x20220000 and a size of 0x20000  it works as expected (for DMA).

2022_dma.jpg

If I choose to start the region at 0x20240000 (size 0x20000), it seems that any writes to the region don't succeed, but no errors are thrown.  Looking in the memory monitor, the locations are all 0x00 (initialized).

2024_dma.jpg

dma_2024_memory_write.jpg

I also make the appropriate changes to the MPU config for the region and the section definition in the linker:

linker_dma.jpg

mpu_2024_dma.jpg

Then I assign the buffer to the DMA region with the following:

DMAMEM_ALIGN( uint8_t buffer[3200], 4);‍‍

with:

#define DMAMEM_ALIGN(var, alignbytes) \
 __attribute__((section(".dmabuffers"))) var __attribute__((aligned(alignbytes)))‍‍‍‍

Again, this all works if the region is at address 0x20220000...

Any ideas?

Labels (2)
0 Kudos
5 Replies

612 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Jack King

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
It seems a bit weird, I'd like to know more information about the phenomenon, so I was wondering if you can share the demo project, in addition, introduce the complete testing process in details.
Looking forward to your reply.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos

612 Views
jackking
Senior Contributor I

Jeremy,

Sure, here are two identical basic projects from MCUXpresso 11.0 that test WRITE/READ to the memory region.

One uses 0x20220000  and the other uses 0x20240000

The one using 0x20240000  fails to read back what was written (memory remains 0x00).

The one using 0x20220000  succeeds.

I am using an Embedded Artists board, so you may need to change the XIP flash driver.

0 Kudos

612 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Jack King

Thanks for your reply.
In the RT series, the FlexRAM is a highly configurable and flexible RAM memory array. This memory array contains
memory banks which can be independently configured to be accessed by a different type of interfaces, such as I-TCM (Instruction-Tightly Coupled Memory), D-TCM (Data- Tightly Coupled Memory), or
AXI (system). The memory bank can act as an ITCM, DTCM, or OCRAM memory.
Table 1 illustrates the different configurations of FlexRAM banks.

pastedImage_6.png
According to Table 1, we can find that the default size of the OCRAM is 256 KB which is equal to 0x40000, so the DMAMEM area is definitely beyond the range of the OCRAM as the Fig 1 shows.

pastedImage_1.png

Fig 1

I think it's the root cause of your issue.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos

612 Views
jackking
Senior Contributor I

That table states that OCRAM can be as large as 384kB, so 0x40000 + 0x20000 should be ok for the total OCRAM size.

EDIT:  Oh WOW... I think I totally misunderstand some fundamental things about FlexRAM...    It looks like the default behaviour is to use the FUSE settings for FlexRAM configuration.  Which is:

flexram__fuse_default.jpg

I thought that changing the MCU settings for memory details in MCUXpresso actually *reconfigured* FlexRAM...  apparently it does NOT

The MCU settings only reconfigure memory within the FlexRAM sizes set by the fuses (by default). 

To change the defined FlexRAM sizes, either the fuses have to be set differently or the FlexRAM has to be explicitly reconfigured in software.

I see that there is an SDK example that shows actually reconfiguring FlexRAM with software, I will try this example and see if I can get past my original issue.  But this fundamental misunderstanding has caused many hours of frustration with other issues as well!

0 Kudos

612 Views
jackking
Senior Contributor I

OK, so I tested again after doing a software reconfiguration of FlexRAM with the following:

static status_t OCRAM_Reallocate(void)
{
    flexram_allocate_ram_t ramAllocate = {
        .ocramBankNum = 12,
        .dtcmBankNum  = 0,
        .itcmBankNum  = 4,
    };

    if (FLEXRAM_AllocateRam(&ramAllocate) != kStatus_Success)
    {
        return kStatus_Fail;
    }

    return kStatus_Success;
}‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

...

#if defined(__DCACHE_PRESENT) && __DCACHE_PRESENT
    SCB_DisableDCache();
#endif
    /* reallocate ram */
    OCRAM_Reallocate();
    /* init flexram */
    FLEXRAM_Init(FLEXRAM);
#if defined(__DCACHE_PRESENT) && __DCACHE_PRESENT
    SCB_EnableDCache();
#endif

This works, although the J-Link debugger fails to connect every second launch when doing this.  I have to wipe the XIP flash and reconnect the debugger to get it working again, then it will fail on the second launch again...   This is using MCUX 11.0.1 and J-Link V651b, but it happens on MCUX 11.0.0 and J-Link V646k as well.

0 Kudos