IMXRT1024 UART Receiver/Transmitter Shift Register Sizes

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMXRT1024 UART Receiver/Transmitter Shift Register Sizes

Jump to solution
775 Views
Lukas_Frank
Senior Contributor I

Hi all,

 

What are the possible sizes of Receiver/Transmitter shift register sizes of UART.

Lukas_Frank_0-1625487976953.png

Is that a true inference that we are able to set sizes of shift registers according to character length? In above figure (from reference manual) Transmit Shift Register is 11-BIT and Receiver Shift Register is 12-BIT? Are these values are just representation between given interval ? [Character Length (7,8,9,10) + Start/Stop Bits  (1,2)]

 

Thanks and Regards.

0 Kudos
1 Solution
764 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @Lukas_Frank,

The representation in the block diagram is only a use case, as it mention in the chapter 44.3.4, the central element of the LPUART transmitter is the transmit shift register that is 9-bitto 13-bit long depending on the setting in the CTRL[M], CTRL[M7], BAUD[M10] and BAUD[SBNS] control bits.

Best Regards,

Alexis Andalon

View solution in original post

1 Reply
765 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @Lukas_Frank,

The representation in the block diagram is only a use case, as it mention in the chapter 44.3.4, the central element of the LPUART transmitter is the transmit shift register that is 9-bitto 13-bit long depending on the setting in the CTRL[M], CTRL[M7], BAUD[M10] and BAUD[SBNS] control bits.

Best Regards,

Alexis Andalon