IMXRT UARTS Hardware RS485 and Smartcard operation

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMXRT UARTS Hardware RS485 and Smartcard operation

861 次查看
gredpath
Contributor III

I am trying to configure the RT10XX families to run RS485 with Hardware flow control and Smartcard operation.

Is this possible with these parts, an initial reading of the datasheet seems to suggest not. 

0 项奖励
2 回复数

685 次查看
gredpath
Contributor III

Thanks Igor for the prompt reply, that answers the first part of the question, I checked this section of the document but I can't find support for ISO7816 smartcards using a UART, is there an app note to point me in the right direction for Smart card support?

Many thanks

George

0 项奖励

685 次查看
igorpadykov
NXP Employee
NXP Employee

Hi George

for rs485 usage one can look at sect.39.2.2.4 Transceiver driver enable

using RTS_B i.MX RT1050 Reference Manual
https://www.nxp.com/docs/en/reference-manual/IMXRT1050RM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励