IMXRT 1064 Access to flexSPI2 pins

cancel
Showing results for 
Search instead for 
Did you mean: 

IMXRT 1064 Access to flexSPI2 pins

150 Views
markomarusic25
Contributor II

I am not sure how to find this information, so maybe someone can help me. Is there a way to physically access  flexSPI2 pins on IMXRT1064? FlexSPI2 peripheral is used for communication between processor and QSPI flash. I am wondering, for security reasons, is this possible or are they connected on silicon inside the chip?

Labels (1)
Tags (2)
1 Reply

54 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

FlexSPI2 pins on IMXRT1064  are just the internal pins, which is not exported on the package. More information you may refer to the application note AN12290.

https://www.nxp.com/docs/en/application-note/AN12290.pdf .

Have a nice day.

 

Best regards

TIC