IMX RT1064 devkit design files

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX RT1064 devkit design files

810 Views
sammypeiren
Contributor I

Hello,

We're currently evaluating the IMX RT 1064 for a camera application. We have the devkit, but unfortunately it only provides an 8-bit video input port. That is, not all of the video input pins are connected to the camera connector.

We were hoping to re-use the devkit design files and modify it slightly so that we get access to all of the pins. This would be a way to quickly evaluate the performance of the IMX RT 1064 with our camera, without having to recreate the entire layout.

The problem is we are using Altium designer and the original design was made using Allegro PCB designer. Importing Allegro files in Altium is possible, but only if:

1) you have Allegro on the same machine

2) or you have the original files in Allegro ASCII format

Since option 1 is not possible for us, I'd like to ask if it would be possible to provide the design files in ASCII format so that we can import them in Altium.

The reference number for this design is: LAY-32221_A

Kind regards,

Sammy

0 Kudos
1 Reply

575 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Sammy,

Unfortunately, we do not have the files in that format. Sorry for the inconvenience that this might cause you.

Have a great day,

TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos