I2S_dma driver 2x24-bits transfer problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I2S_dma driver 2x24-bits transfer problem

Jump to solution
6,460 Views
slawek_zabielsk
Contributor III

Starting from evkmimxrt685_i2s_dma_record_playback sample project with SDK, I try to run the same audio sampling functionality by codec WM8904, but not in 16 bits, but in 24 bits (2channels, 48kHz). I managed to get the situation where codec itself works in 24 bits. But the DMA transfer only allows me to transfer one channel. (one channel mode, MONO) When I turn on second channel (STEREO) DMA sends me only half of data (probably I get every second sample). Can the I2S_dma driver only transfer 32 bits from FIFO to my buffer? But is there any way to send 2x 32 bits each?
I have the same problem with I2S_dma if you use 48-bits packed option (2x24bits). I get every second sample.

Labels (1)
Tags (1)
0 Kudos
1 Solution
6,084 Views
slawek_zabielsk
Contributor III

Hi Kerry. Indeed, taking the data from the debugger window directly, the results are correct. No zeros. Pure triangle waveforms. It looks like the problem really lies in the printf function. Hence, the conclusions were wrong. The sample project with 24-bit 2 channels after my amendment works correctly! I close the thread. Thank you for help.

View solution in original post

0 Kudos
15 Replies
6,365 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi adrian_klimczak,

    Thanks so much for your detailed reply and the code, and sorry for my later reply!

     I also checked your code and test it on my side.

    You mentioned that: we get half data for left and half data for right channel

    But from the test result:

image.png

Take the data as an example:

L: 51,255,255,0;  = 0XFFFF33

R:33,254,255,0;  = 0XFFFE21

L:243,253,255,0; = 0XFFFDF3

R:121,253,255,0;= 0XFFFE79

All the related channel is 24bit, could you tell me why you mention:  get half data for left and half data for right channel?

From the result, it is the 24 bit, not just half data.

Sorry, I still don't very clear about your question details,  do you want the DMA send your just 24bits data directly, instead of the 32bit which also contains one byte 0X00?

Best Regards,

Kerry

    

0 Kudos
6,361 Views
adrian_klimczak
Contributor II

Thank you for your reply. 

What you are stating is correct, but this is not the issue we are experiencing. Let me try to elaborate a bit more about the issue we are experiencing. 

 

What you are showing us on your image is the first part of the signal, which is valid. If you look at the last part of the buffer, it would be lots of zeros.

0,0,0,0,
0,0,0,0,
0,0,0,0,
0,0,0,0,
0,0,0,0,
0,0,0,0,
0,0,0,0,

If you look at the attached "Screenshot 2020-10-20 at 16.56.42.png" in one of my replies, you will see that about half of the samples (50 samples) give three triangles (triangular signal) and from about sample 51st to sample 100th samples are flat with some small anomalies, while it should continue with the triangular signal.

Our signal comes from function generator, using triangular wave.

Buffer is 100 samples per channel (int32 values) -> 4 bytes per sample (400 uint8 values) per channel = 800 uint8 values in total for 2 channels. First 4 bytes is left channel then 4 bytes for right channel.

For example:

29,81,231,0, // Left Channel
86,34,173,0, // Right Channel
181,232,203,0, // Left Channel
164,219,204,0, // Right Channel

Please look at the second half of the buffer to verify that it has lots of zeros. Can you see those zeroes? If not, what is your input, is it function generator, wav file, static array?

Screenshot 2020-10-30 at 09.14.57.png

0 Kudos
6,341 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi adrian_klimczak,

  So sorry for my later reply, really a lot of cases in the testing queue.

   I didn't add any input source when I test your project in the last time.

   Thanks for letting me know that your input the triangular wave, could you please tell me your detail triangular wave from your function generator? 48Khz? Can you give me your photo about your input triangular wave? I will also find one function generator and test it like you. 

   Please also let me know your wave connection to the RT685-EVK board, and give me the photo.

   I need to test it, and try to reproduce your issues, then I can check more detail with our expert.

   Please let me know more details to reproduce your issues, the board connection with your signal source input, and your input source details, amplitude and the frequence.

 

Best Regards,

Kerry

0 Kudos
6,327 Views
slawek_zabielsk
Contributor III

Hi Kerry.

We use a normal function generator which is connected directly to the MIMXRT685-EVK devboard, via J3 connector. Parameters of the signal from generator:
1. Triangle mode,
2. output voltage 1.4Vpp,
3. frequency 375Hz.
At the input (J3) and output (J4) of the devboard, I connect an oscilloscope probe for viewing. (ch1.output signal, ch2.input signal) I attach a sample oscillogram of such measurement.
Best Regards,
Slawek

0 Kudos
6,301 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi  slawek_zabielsk,

   When you use the generator Triangle mode generate the wave, then it will output 2 wire, GND, and the wave from the generator, how you connect it to the J3?

image.png

How do you connect the signal between the generator and the J3?

Because I don't have the connector, then I need to connect the generator two-pin to the EVK circuit directly. Then I want to know your detailed connection and I can test it.

Best Regards,

Kerry

0 Kudos
6,299 Views
slawek_zabielsk
Contributor III

Hi Kerry.

I connect the generator via my Scarlet 2i2 sound card. Then I connect the output of the card to the devboard input. To do this I use two cables:
1. Coaxial -> JACK 1/2" - connection of the generator output with input 1 of the music card
2. JACK 3.5mm plug -> JACK 3.5mm plug - connection of the sound card output with NXP devboard input (J3)
Since the music card output is JACK 1/2" socket, I additionally use a 1/2" JACK adapter on the 3.5mm JACK shown in the picture. I connect the oscilloscope probe to the devboard output using a second cable type 2.

IMG_20201106_100449.jpg

Best Regards,

Slawek

0 Kudos
6,193 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi slawek_zabielsk,

   I don't have your test wire, I just have these tools and wire:

1.jpg3.jpg

So, if I need to use the function generator tool, I may need to input two channel, then connect one signal to LININL_JACK, another to LININR_JACK.

Could you please give me your oscilloscope wave in LININL_JACK and LININR_JACK?

image.png

Today, I borrow one following 3.5mm wire from my colleagues in the other department:

2.jpg

Then use the PC to connect this wire, and connect to the board J3, and play the music, I also use the headphone to connect J4 to hear the loopback.I find the music is correct, but your printf data is really still have the issues that half data is 0, but the song should no so much 0s, So I still need to check the detail reason with our internal side, maybe I still also need to check input the directly fixed wave, then printf the data, and then talk with our internal expert about your issues

Now, please share me your oscilloscape wave about two channel, one channel is LININL_JACK, another channel is LININR_JACK, I will also try to test the same wave.

The following is my test result with the music:

Configure WM8904 codec

Configure I2S

Setup digital loopback

212,185,255,0;

92,69,0,0;

58,162,255,0;

64,10,0,0;

41,238,255,0;

2,255,255,0;

198,47,0,0;

174,27,0,0;

194,166,0,0;

155,69,0,0;

51,202,0,0;

77,160,0,0;

252,235,0,0;

164,219,0,0;

104,233,0,0;

66,190,0,0;

193,128,0,0;

254,146,0,0;

44,44,0,0;

167,41,0,0;

84,19,0,0;

70,33,0,0;

149,33,0,0;

128,4,0,0;

158,17,0,0;

168,199,255,0;

103,237,255,0;

146,167,255,0;

228,241,255,0;

173,139,255,0;

234,220,255,0;

133,118,255,0;

109,125,255,0;

20,254,254,0;

34,82,255,0;

112,174,254,0;

215,55,255,0;

129,163,254,0;

110,38,255,0;

191,159,254,0;

99,74,255,0;

47,62,255,0;

104,30,255,0;

143,255,254,0;

175,217,254,0;

255,196,254,0;

97,251,254,0;

168,183,254,0;

112,235,254,0;

108,163,254,0;

102,195,254,0;

201,204,254,0;

241,209,254,0;

43,3,255,0;

116,161,254,0;

232,42,255,0;

19,172,254,0;

87,88,255,0;

247,246,254,0;

155,128,255,0;

164,16,255,0;

84,175,255,0;

141,254,254,0;

93,83,255,0;

114,151,255,0;

19,193,255,0;

161,159,255,0;

96,216,255,0;

224,181,255,0;

188,17,0,0;

229,158,255,0;

8,16,0,0;

217,121,255,0;

168,217,255,0;

27,136,255,0;

62,140,255,0;

19,107,255,0;

241,147,255,0;

197,95,255,0;

71,130,255,0;

227,106,255,0;

178,180,255,0;

188,115,255,0;

34,231,255,0;

95,141,255,0;

123,208,255,0;

10,142,255,0;

66,188,255,0;

33,116,255,0;

84,113,255,0;

234,159,255,0;

165,90,255,0;

186,211,255,0;

212,116,255,0;

254,210,255,0;

164,129,255,0;

95,226,255,0;

13,184,255,0;

144,159,255,0;

93,131,255,0;

225,119,0,8;

176,28,8,0;

225,119,0,8;

64,28,8,0;

0,0,0,0;

0,0,0,0;

4,1,0,0;

3,0,0,0;

64,0,0,0;

4,0,0,0;

27,113,0,8;

40,26,8,0;

0,0,0,0;

48,19,8,0;

40,3,0,0;

48,19,8,0;

2,0,0,0;

4,0,0,0;

128,25,8,0;

48,19,8,0;

40,3,0,0;

48,19,8,0;

0,0,0,0;

0,2,0,0;

48,19,8,0;

40,3,0,0;

80,11,8,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,54,110,1;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,112,16,64;

240,25,8,0;

1,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

0,0,0,0;

 

0 Kudos
6,172 Views
slawek_zabielsk
Contributor III

Hi Kerry,

I am enclosing the oscilloscope waveforms in LININL_JACK and LININR_JACK in a file.

So far we got the same results as you.

Best Regards,

Slawek

0 Kudos
6,107 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi slawek_zabielsk,

   Seems the printf result have issues, do you debug your code, and check the s_Buffer_copy array data directly?

   I find there are not so much 0s.

 
0 Kudos
6,085 Views
slawek_zabielsk
Contributor III

Hi Kerry. Indeed, taking the data from the debugger window directly, the results are correct. No zeros. Pure triangle waveforms. It looks like the problem really lies in the printf function. Hence, the conclusions were wrong. The sample project with 24-bit 2 channels after my amendment works correctly! I close the thread. Thank you for help.

0 Kudos
6,416 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi adrian_klimczak,

  Please share me your modified project directly, and let me know your testing IDE, I need to test it directly and check it on my side.

  Please also tell me how do you get your attached pictures?

 

Best Regards,

Kerry

 

6,409 Views
adrian_klimczak
Contributor II

Hi kerryzhou,

Thank you for your quick response.

Please, see the modified sample project attached: evkmimxrt685_i2s_dma_record_playback.zip.

We are using MCUExpresso IDE.

To get the attached picture:

  • In i2s_dma_record_playback.c
    • Line 225: We print to the Console the rx data uint8 values stored in s_Buffer_copy variable.
    • Then, we copy these printed values to .txt file. We replace ; with.
    • Then we copy these values from .txt file to our C++ code, which does conversion of three bytes into int32 samples. We print these samples to the console. (please see test_code.c attached, it's c++ code, but I have to attach it as .c file)
    • We use tutorialspoint.com/compile_cpp_online.php to quickly execute our test code.
    • Then we copy those samples to excel spreadsheet to create a graph.

Changes we made to sample project:

  • source/i2s_dma_record_playback.c
    • .bitWidth = kWM8904_BitWidth16 -> 

      .bitWidth = kWM8904_BitWidth24

    • #define DEMO_AUDIO_BIT_WIDTH (16) -> #define DEMO_AUDIO_BIT_WIDTH (24)

    • #define DEMO_I2S_CLOCK_DIVIDER 16 -> #define DEMO_I2S_CLOCK_DIVIDER 8

  • drivers/fsl_i2s.c (Line 218 and 272)
    • config->dataLength = 16U; -> config->dataLength = 24U;

    • config->frameLength = 32U; ->  config->frameLength = 64U;
  • codec/fsl_wm8904.c (Line 85)
    • result = WM8904_ModifyRegister(handle, WM8904_AUDIO_IF_1, 0x000C | (1U << 6U), format->bitWidth); ->  result = WM8904_ModifyRegister(handle, WM8904_AUDIO_IF_1, 0x000C | (1U << 6U), (format->bitWidth)<<2u);

Please, let me know if your require any more information.

 

0 Kudos
6,449 Views
adrian_klimczak
Contributor II

We are working with Slawek on the same project in the same team, therefore let me fill the details to help us receive an answer to this problem.

In order to get 24 bits for just one channel we did the following modifications to the "evkmimxrt685_i2s_dma_record_playback" sample project:

  • we changed Bit Width from 16 bit to 24.
  • we changed clock divider from 16 to 8.
  • config->oneChannel from false to true.
  • config->dataLength from 16 to 24.
  • config->frameLength from 32 to 64.

After doing these changes we noticed that we still get 16 bit data length values, therefore we modified fsl_wm8904.c file, line 85,

from

result = WM8904_ModifyRegister(handle, WM8904_AUDIO_IF_1, 0x000C | (1U << 6U), format->bitWidth);

to 

result = WM8904_ModifyRegister(handle, WM8904_AUDIO_IF_1, 0x000C | (1U << 6U), (format->bitWidth)<<2u);

After this change, we started receiving 24 bit length data however just for one channel. If we set:

config->oneChannel = false

Then, we get half data for left and half data for right channel. Please see attached .png file.

Are we configuring something wrong?

6,429 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi adrian_klimczak,

   Please send me your modified project directly, I need to check your code details, whether you modified the correct points.

Best Regards,

Kerry

0 Kudos
6,433 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi All,

  Sorry for the later reply.

   Please give me more time to analyze your issues, I will give your feedback ASAP, please keep patient, thanks.

Best Regards,

Kerry