Dears,
I want to understand I2C communication on RT1052. So, I transfer the SDK example: lpI2c_interrupt.c. Please would like to know if the IMXRT1050-EVKB Evaluation Kit is capable of running this example and simulating I2C communication. If the Kit is capable of simulating communication, I would like to know which element will be the master and which element will be the slave.
Best Regards,
Rubens Júnior
Solved! Go to Solution.
Hi Rubens Junior ,
Of course, you can, you can use this SDK i2c code:
SDK_2.6.1_EVKB-IMXRT1050\boards\evkbimxrt1050\driver_examples\lpi2c\interrupt
And test it in the MIMXRT1050-EVKB board, this project already support both I2C master and slave
You just need to do the following setting:
To make lpi2c example work, connections needed to be as follows:
LPI2C1 SCL(J23-6) --> LPI2C3 SCL(J22-1)
LPI2C1 SDA(J23-5) --> LPI2C3 SDA(J22-2)
Then,after you download the code, you can find the printf data:
~~~~~~~~~~~~~~~~~~~~~~~~~~~~
LPI2C example -- MasterFunctionalInterrupt_SlaveFunctionalInterrupt.
Master will send data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
This time , slave will send data:
0xff 0xfe 0xfd 0xfc 0xfb 0xfa 0xf9 0xf8
0xf7 0xf6 0xf5 0xf4 0xf3 0xf2 0xf1 0xf0
0xef 0xee 0xed 0xec 0xeb 0xea 0xe9 0xe8
0xe7 0xe6 0xe5 0xe4 0xe3 0xe2 0xe1 0xe0
Master received data :
0xff 0xfe 0xfd 0xfc 0xfb 0xfa 0xf9 0xf8
0xf7 0xf6 0xf5 0xf4 0xf3 0xf2 0xf1 0xf0
0xef 0xee 0xed 0xec 0xeb 0xea 0xe9 0xe8
0xe7 0xe6 0xe5 0xe4 0xe3 0xe2 0xe1 0xe0
you can try it on your side.
If you still have questions, please kindly let me know.
Have a great day,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi Rubens Junior ,
Of course, you can, you can use this SDK i2c code:
SDK_2.6.1_EVKB-IMXRT1050\boards\evkbimxrt1050\driver_examples\lpi2c\interrupt
And test it in the MIMXRT1050-EVKB board, this project already support both I2C master and slave
You just need to do the following setting:
To make lpi2c example work, connections needed to be as follows:
LPI2C1 SCL(J23-6) --> LPI2C3 SCL(J22-1)
LPI2C1 SDA(J23-5) --> LPI2C3 SDA(J22-2)
Then,after you download the code, you can find the printf data:
~~~~~~~~~~~~~~~~~~~~~~~~~~~~
LPI2C example -- MasterFunctionalInterrupt_SlaveFunctionalInterrupt.
Master will send data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
This time , slave will send data:
0xff 0xfe 0xfd 0xfc 0xfb 0xfa 0xf9 0xf8
0xf7 0xf6 0xf5 0xf4 0xf3 0xf2 0xf1 0xf0
0xef 0xee 0xed 0xec 0xeb 0xea 0xe9 0xe8
0xe7 0xe6 0xe5 0xe4 0xe3 0xe2 0xe1 0xe0
Master received data :
0xff 0xfe 0xfd 0xfc 0xfb 0xfa 0xf9 0xf8
0xf7 0xf6 0xf5 0xf4 0xf3 0xf2 0xf1 0xf0
0xef 0xee 0xed 0xec 0xeb 0xea 0xe9 0xe8
0xe7 0xe6 0xe5 0xe4 0xe3 0xe2 0xe1 0xe0
you can try it on your side.
If you still have questions, please kindly let me know.
Have a great day,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Dear kerryzhou,
The bellow scheme connection it is correct for the evkbimxrt1050_lpi2c_interrupt sample. Please could you tell me wich scheme is required to test the lpi2c_interrupt_b2b_transfer_master and lpi2c_interrupt_b2b_transfer_slave samples.
Have a great day!
Rubens Júnior
Hi Rubens Junior,
You can check the readme in the lpi2c_interrupt_b2b_transfer_master and lpi2c_interrupt_b2b_transfer_slave project:
Hardware requirements
=====================
- Mini/micro USB cable
- Two EVKB-IMXRT1050 board
- Personal Computer
Board settings
==============
LPI2C one board:
+ Transfer data from MASTER_BOARD to SLAVE_BOARD of LPI2C interface, LPI2C1 pins of MASTER_BOARD are connected with
LPI2C1 pins of SLAVE_BOARD
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
MASTER_BOARD CONNECTS TO SLAVE_BOARD
Pin Name Board Location Pin Name Board Location
LPI2C1_SCL J23-5 LPI2C1_SCL J23-5
LPI2C1_SDA J23-6 LPI2C1_SDA J23-6
GND J24-7 GND J24-7
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
So, you need to use two board to these the master and slave.
Wish it helps you!
Have a great day,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Thank you kerryzhou! It's work fine!