I.mxRT GPIO max sinking & sourcing current

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.mxRT GPIO max sinking & sourcing current

1,157 Views
HeMyFAE
NXP Employee
NXP Employee

Dear i.mxRT,

One of my medical  customers who is using a RT64 is also looking for the GPIO max sinking and sourcing current specification for documentation purposes. Please let me know where I can find this info.

I searched in both the DS and RM but there are no such data. Please advise!

Regards,

hy

0 Kudos
1 Reply

1,005 Views
Yuri
NXP Employee
NXP Employee

Hello,

  GPIO DC parameters in i.MX Datasheet(s) provide typical Ioh and Iol values. 

Generally the GPIO drive current is affected by the configuration of the buffer. Customers

can use  DSE field in the controlling IOMUX registers to set the drive strength. There are also
a slew rate controls in those registers which may also have an effect

 The best way to estimate currents is to use the IBIS model for the IO(s) you care about.

IBIS file shows tables with the buffer drive current across a range of pad voltages. You can look

through the list to find the current at the voltage of interest.

  Note, that the IBIS model covers a wider range than the conditions allowed in the datasheet so

not everything in the IBIS model is an allowed use case. Also, these currents in a real case would

be transient lasting only nanoseconds or less. This does not imply you could run the buffer at that

current for an extended period of time.That would cause overheating on the part and create reliability

problems.

 

     i.MX RT 1064 Datasheets contain “GPIO output buffer average impedance” tables. Parameter Output

Driver Impedance allows to estimate

1) max possible (short circuit) current, as following: I = Vout / Impedance   (143 mA =3.3V / 23 Ohm);

2) real current, depending on external load; I = Vout / (Impedance+R_load),  so to get 10mA, external

    load of ~300 Ohm  is needed, assuming DSE =111.

 

  Of course it is needed to  take into account thermal considerations in order to avoid device damage.  

  Also: 

Maximum output current io pin 

Regards,

Yuri.