I.MXRT1011 SPDIF Receiver just up to 88.2 kHz

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I.MXRT1011 SPDIF Receiver just up to 88.2 kHz

1,265 次查看
emagnioj
Contributor II

Hello, on the eval I.MXRT1011 i enabled the S/PDIF receiver but it locks just up to 88.2 kHz 

How to lock spdif receiver at 96 kHz or 176.4 kHz

Thank you!

 

0 项奖励
6 回复数

1,101 次查看
emagnioj
Contributor II

hello  a colleague solved the problem setting IPG_CLOCK_ROOT to 125 MHz and now spdif receiver works up to 192 kHz

thank you!

1,252 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi,

Could you please provide how are you testing this to see if I can replicate this on my side? Please note input frequency range and implications.

FelipeGarcia_0-1618591505308.png

Best regards,

Felipe

0 项奖励

1,242 次查看
emagnioj
Contributor II

Hello Felipe, I got an external S/PDIF TX and connected the output on pin 6 - GND of T1 (not present ) see schematic SPF-45852_c.pdf then jumped J35 and J36.

Then assigned SPDIF IN of the eval board at GPIO_10.

When i send music i see the locked bit asserted SPDIF-SRPC (Phase config register) and i can get back the music from SPDIF OUT pin 6 - gnd of T2 ( not present ).

At 96 kHz and more the SPDIF-SRPC reports no lock and i cannot get back music.

Thank you!

Emag

 

0 项奖励

1,212 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi Emag,

Thank you for your reply. This has already been escalated with the RT applications team, I will provide an update as soon as there is some feedback.

Best regards,

Felipe

0 项奖励

1,180 次查看
emagnioj
Contributor II

Thank you Felipe! Any news?

Best regards,
Emag

0 项奖励

1,170 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi Emag,

The appropriate team has been contacted for testing and analysis, any update I will let you know.

Regards,

Felipe

0 项奖励