Hi guys,
Can I use Hyperram and Hyperflash at the same time with the i.MXRT1062?
I'm planning to connect them as follows:
Hyperram will be connected to FLEXSPI2 using eight data channels
HyperFlash will be connected to FLEXSPI using eight data channels
Thanks!
Hello,
>>Can I use Hyperram and Hyperflash at the same time with the i.MXRT1062?
Yes. RT1062 can support it. Hope it help you. Have a nice day.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------