Hyper Flash on IMX RT1060-EVK does not work

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hyper Flash on IMX RT1060-EVK does not work

3,525 Views
pjanco
Contributor III

Hi,

I have MIMXRT1060-EVK Rev.A2 board and onboard Hyperflash 6KS512SDP does not work.

I am using latest MCUXpresso IDE v10.3.0.

SDK_2.x_EVK-MIMXRT1060 v2.5.0.

I already removed resistors R153,R154,R155,R156,R157,R158 and mounted resistors R356,R361,R362,R363,R364,R365,R366.

SW7 is in position for hyperflash - OFF,ON,ON,OFF.

I am not sure if R169 should be mounted or not. I tried both options, with the same result.

I also regunfigured memory areas like this:

memory.jpg

It shows me this error after start debug using link server:

link_server.jpg

I also try to reconfigure SW7 to serial downloader and then do Mass erase procedure:

serial_downloader.jpg

I also try external debugger J-link with similar result. Where is the problem? Do anyone have onboard HyperFlash functional? I have also other board IMXRT1050-EVKB and there Hyperflash is working well by default.

6 Replies

2,720 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Peter,

    1. Hardware

       OPTION1: USE Hyperflash( DNP R153~R158, Mount R356,R361~R366)
      OPTION2: USE QSPI FLASH(Mount R153~R158, DNP R356,R361~R366)

      Please double check your solder, make sure it is correct.

   2. Software

       Your configuration is not enough, you need to modify the evkbimixrt1060_flexspi_nor_config.c ,

       Comment these code:

const flexspi_nor_config_t qspiflash_config = {
    .memConfig =
        {
            .tag = FLEXSPI_CFG_BLK_TAG,
            .version = FLEXSPI_CFG_BLK_VERSION,
            .readSampleClkSrc = kFlexSPIReadSampleClk_LoopbackFromDqsPad,
            .csHoldTime = 3u,
            .csSetupTime = 3u,
            // Enable DDR mode, Wordaddassable, Safe configuration, Differential clock
            .sflashPadType = kSerialFlash_4Pads,
            .serialClkFreq = kFlexSpiSerialClk_100MHz,
            .sflashA1Size = 8u * 1024u * 1024u,
            .lookupTable =
                {
                    // Read LUTs
                    FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0xEB, RADDR_SDR, FLEXSPI_4PAD, 0x18),
                    FLEXSPI_LUT_SEQ(DUMMY_SDR, FLEXSPI_4PAD, 0x06, READ_SDR, FLEXSPI_4PAD, 0x04),
                },
        },
    .pageSize = 256u,
    .sectorSize = 4u * 1024u,
    .blockSize = 256u * 1024u,
    .isUniformBlockSize = false,
};‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

Add these code:

  

const flexspi_nor_config_t hyperflash_config = {
    .memConfig =
        {
            .tag = FLEXSPI_CFG_BLK_TAG,
            .version = FLEXSPI_CFG_BLK_VERSION,
            .readSampleClkSrc = kFlexSPIReadSampleClk_ExternalInputFromDqsPad,
            .csHoldTime = 3u,
            .csSetupTime = 3u,
            .columnAddressWidth = 3u,
            // Enable DDR mode, Wordaddassable, Safe configuration, Differential clock
            .controllerMiscOption =
                (1u << kFlexSpiMiscOffset_DdrModeEnable) | (1u << kFlexSpiMiscOffset_WordAddressableEnable) |
                (1u << kFlexSpiMiscOffset_SafeConfigFreqEnable) | (1u << kFlexSpiMiscOffset_DiffClkEnable),
            .sflashPadType = kSerialFlash_8Pads,
            .serialClkFreq = kFlexSpiSerialClk_133MHz,
            .sflashA1Size = 64u * 1024u * 1024u,
            .dataValidTime = {16u, 16u},
            .lookupTable =
                {
                    // Read LUTs
                    FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0xA0, RADDR_DDR, FLEXSPI_8PAD, 0x18),
                    FLEXSPI_LUT_SEQ(CADDR_DDR, FLEXSPI_8PAD, 0x10, DUMMY_DDR, FLEXSPI_8PAD, 0x06),
                    FLEXSPI_LUT_SEQ(READ_DDR, FLEXSPI_8PAD, 0x04, STOP, FLEXSPI_1PAD, 0x0),
                },
        },
    .pageSize = 512u,
    .sectorSize = 256u * 1024u,
    .blockSize = 256u * 1024u,
    .isUniformBlockSize = true,
};‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

3. Before you download the code

   Please note this point:

pastedImage_2.png

Then try to download the code to your chip, after you download it, you modify SW7_2 ON, SW7_3 ON, SW7_1 OFF, SW7_4 OFF, just run the code from the external hyper flash.

Please try it, actually this is the same as the RT1050-EVKB board.

More details, please refer to this application note:

https://www.nxp.com/docs/en/application-note/AN12107.pdf 

If you still have question about it, please kindly let me know.

       


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,720 Views
pjanco
Contributor III

Hi, it is working with modified ".memConfig". But I still have the same error as in my printscreen while using serial downloader mode.

I figure out:

It is working well with driver "MIMXRT1050-EVK_S26KS512S.cfx" even on "1060" board.

Driver MIMXRT1060_SFDP_HYPERFLASH.cfx" does not work.

What is this driver doing?
Does this driver have any effect if I use SWD connection instead of serial downloader?

If I try to erase flash on "MIMXRT1062XXX6A" device using Jlink commander, it give me this error:

J-Link>exec EnableEraseAllFlashBanks
J-Link>erase
Erasing device...
J-Link: Flash download: Total time needed: 0.203s (Prepare: 0.154s, Compare: 0.000s, Erase: 0.048s, Program: 0.000s, Verify: 0.000s, Restore: 0.000s)

****** Error: Failed to erase sectors 0 @ address 0x60000000 (erase error)
ERROR: Erase returned with error code -5.‍‍‍‍‍‍‍‍‍‍‍‍‍‍

I tried to manually set device "MIMXRT1052XXX6A", even If  I use "MIMXRT1062XXX6A". With this settings the "erase" procedure is working.

By the way, how can I add "exec EnableEraseAllFlashBanks" while using "jlink/erase" button in MCUExpresso?

Regards,

Peter.

0 Kudos

2,720 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Peter,

    Thanks a lot for your updated information.

    I have checked the RT1050 sdk code, RT1050 board is using the hype flash in default, I find the SDK code is also using MIMXRT1050-EVK_S26KS512S.cfx, not the MIMXRT1050-SFDP_HYPERFLASH.cfx.

    pastedImage_1.png

So, you can use the MIMXRT1050-EVK_S26KS512S.cfx at first, when I have time, I will check the details about the MIMXRT1060-SFDP_HYPERFLASH.cfx,maybe it need to check the according source code.

About the erase all the external flash, I think, you can use the JLINK commander to erase it:

pastedImage_2.png

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

2,720 Views
Takashi_Kashiwagi
Senior Contributor I

Hi Peter.

Did you modified XXXX_flexspi_nor_config.c in xip? There are some diffrerent code between QSPI Flash and HyperFlash.

diff.png

Please Chechk xip foleder in your project (1050-EVKB and 1060-EVK).

Best Regards,

T.Kashiwagi

2,720 Views
pjanco
Contributor III

Hi, now it is working.

Thanks!

2,720 Views
PavelM
NXP Employee
NXP Employee

My customer reported the same...

0 Kudos