How to use the QSPI flash in Gui-Guider with imxrt1050?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use the QSPI flash in Gui-Guider with imxrt1050?

Jump to solution
1,025 Views
mperez1
Contributor II

Hello there,

I just discover the Gui-Guider application to use with lvgl. I'm able to generate a project and add widgets. But my problem is when i'm trying to load the application in the board. I have a custom board with a QSPI flash instead of a Hyperflash. There is any way to change this in the Gui-Guider? Even changing any file in the Gui-Guider root?

Thank you in advance,

Miguel

0 Kudos
Reply
1 Solution
1,008 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Miguel,

Booting from QSPI depends on the project configuration. The MCUXpresso SDK example is intended to boot from Hyperflash, please check the following application note for more details.

https://www.nxp.com/docs/en/nxp/application-notes/AN12183.pdf

Best regards,

Felipe

View solution in original post

0 Kudos
Reply
1 Reply
1,009 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Miguel,

Booting from QSPI depends on the project configuration. The MCUXpresso SDK example is intended to boot from Hyperflash, please check the following application note for more details.

https://www.nxp.com/docs/en/nxp/application-notes/AN12183.pdf

Best regards,

Felipe

0 Kudos
Reply