Hi,
I want to test the USB bandwidth in RT1050, from
https://www.freesion.com/article/8561135712/#_263
has some information about it, but the attached files can not download anymore.
1) I need to setup the example to do USB test, is SDK example evkbimxrt1050_dev_hid_mouse_freertos a suitable USB performance test example?
2) evkbimxrt1050_dev_hid_mouse_freertos has the "Interrupt In" only, how can I modify the example to have "Bulk Out" for USB performance test?
Hi @felix1
I'll look into the link you share, however, any USB example could be usefull to do the performance test and I don't see a problem with the"Interrupt In" still I will see if there is any other example that aproaches to a bulk-out test.
Best Regards, Miguel.
Hi @Miguel04 ,
I need to make sure RT1050 USB can meet our project to capture physiological signal data, otherwise I need to change another MCU.
Any method to measure RT1050 USB performance is welcome.
Hi,
AN13474 test method is too complex and need equipment like Oscilloscope Keysight DSOS604A.
For now I think write a C# AP (use LibUsbDotNet) to test RT1050 USB performance should be enough for our need.