How to get the *.mex from MDK's project?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to get the *.mex from MDK's project?

647 次查看
cody1
Contributor III

I saw board.c, board.h, clock_config.c... and so on

in the SDK_2.6.1_EVKB-IMXRT1050\boards\evkbimxrt1050\driver_examples\gpio\led_output.
These files seem to make from MCUXpresso Config Tools, but I can't find the file *.mex in this folder.

标签 (1)
0 项奖励
1 回复

602 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hello Cody,

 

Not all the examples contain a *.mex file already in the project. You can find some in this folder:

SDK_2.7.0_EVKB-IMXRT1050_MDK\boards\evkbimxrt1050\demo_apps

For more information I highly recommend you to refer to the MCUXpresso Config Tools User Guide.

 

Have a great day,
Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励