How to flash an .hex file into the i.MX RT1020 EVK?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to flash an .hex file into the i.MX RT1020 EVK?

1,230 次查看
arimendes
Contributor III

Hi,

 What tools can I use to load a .hex file into the i.MX RT1020 EV and run the code?

0 项奖励
2 回复数

1,163 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To provide the fastest possible support, I'd highly recommend you use the NXP-MCUBootUtility which is a GUI tool specially designed for NXP MCU secure boot. Its features correspond to the BootROM function in NXP MCU.
Please give a try.
https://github.com/JayHeng/NXP-MCUBootUtility

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励

1,147 次查看
pholden
Contributor II

Is there a flash programming tool that runs on Linux?

0 项奖励