Hi all,
I am working on custom board using MIMXRT1052CVL5B, and flash W25Q256JV. This board connect W25Q256JV according to image bellow:
My question: "How to boot from W25Q256JV".
Thanks for your help.
Solved! Go to Solution.
Thanks for your reply,
This problem is solved.
i have configured "Flash_Type" and "BT_FUSE_SEL":
Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) How to boot from W25Q256JV?
-- The hardware connection seems right, you can use the tool to MCUBootUtility tool program an application image to above QSPI, then set the corresponding boot pin or eFuse bit to boot from the flash.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Thanks for your reply,
This problem is solved.
i have configured "Flash_Type" and "BT_FUSE_SEL":