GPIO Output to Output Skew

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GPIO Output to Output Skew

Jump to solution
678 Views
ccrsa
Contributor I

Hi

I was wondering if it is possible to use the RT1064 GPIO to synchronously trigger external counters  instead of using pin fanout or a 1-to-4 clock buffer. 

What would be the output-to-output skew between GPIO output pins controlled by the same DR? 

Thank you.

C

Labels (1)
0 Kudos
1 Solution
645 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @ccrsa ,

If the two GPIOs are in same group, there will be no difference because you can toggle them in a same register at same time. There isn't hardware path difference for them.

 

Regards,

Jing

View solution in original post

0 Kudos
3 Replies
670 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @ccrsa ,

I'm not very clearly understand your requirement. But I think you can use the RT1060 XBAR function.

 

Regards

Jing

0 Kudos
663 Views
ccrsa
Contributor I

Thank you for responding @jingpan.

Sorry if I was not clear. What I meant was if you toggled 2 x GPIO outputs from low to high and compared the signal transitions with an oscilloscope, would there be a significant time delay or skew between them and would it be deterministic? 

0 Kudos
646 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @ccrsa ,

If the two GPIOs are in same group, there will be no difference because you can toggle them in a same register at same time. There isn't hardware path difference for them.

 

Regards,

Jing

0 Kudos