FlexSPI control NORFLASH

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FlexSPI control NORFLASH

1,107件の閲覧回数
zhangyanming
Contributor I

Lately, i use i.MX RT 1052 to do a project.In the project,i want to use the FlexSPI to control two same NORFLASH,one is
controllede by portA ,i wang to use this to storage code,the code is implemented in XIP mode.the other one is controlled by
portB,i want to use this to storage data.Now,the question is one FlexSPI can realize this function?If it is feasible,how to
realize?If it is not feasible,why?
thanks.

ラベル(1)
0 件の賞賛
1 返信

927件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

   It is possible to use the i.MX RT1050  FlexSPI channels A and B separately. 

You may look at section 30.7.3 (Flash Connection) of i.MX RT1050 Reference Manual (RM),

Rev. 1, 03/2018.

  I am afraid we do not have an example just for such case. Use section 30.8 (Application information)

of the RM.

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 件の賞賛